Click here to return to the Basic page
The parameter Read module can be used to read any parameter in the schematic and get the value in the output pin.
The parameter Write block allows user to update the module's parameter value dynamically. The selected parameters are updated with the value coming from the input pins
The selection of the parameter will be enabled only when the schematic compilation is completed successfully. The user can select the module for which the parameter needs to be updated/Read. After selecting the module, the parameter within the module should be selected for which value should be updated. The value of the selected parameter will be updated with the given input value for each sample once the schematic is downloaded. User can also change the parameter selection when the schematic is downloaded. It will start updating/Read the newly selected parameter once the parameter selection window is closed.
Name | ADSP-214xx | ADSP-215xx/SC5xx | ADAU145x/146x |
---|---|---|---|
—————————— | ——————-- | ——————————-- | —————————- |
Param Read | B | B | NA |
Param Write | B | B | NA |
Name | Type | Description |
---|---|---|
———————- | ————-- | ———————- |
Input | Control | Input Channel (Only for ParamWrite) |
Name | Type | Description |
---|---|---|
———————- | ————-- | ———————- |
Output | Control | Output Channel (Only for ParamRead) |
GUI Parameter | Default Value | Range | Function Description |
---|---|---|---|
—————————————- | ———————- | —————— | —————————————- |
Module | NA | NA | Name of the module in the schematic |
Parameter | NA | NA | Name of the parameter in the selected module |
Address | 0 | NA | Address of the parameter. If the user wants to enter the address directly Select the Address mode |
Mode | Parameter | Parameter / Address | User can select the mode |
Format | Float | Float / Int32 | Data type of the parameter |
Parameter Name | Description | ADSP-214xx/SC5xx/215xx | ADAU145x/146x |
---|---|---|---|
—————————————- | ———————————————————————————————————- | —————————- | —————— |
Address | Address of the parameter | Integer32 | NA |
Offset | This offset is added to the address, then that is used as the address to read the parameter from | Integer32 | NA |
Type | Data type of the parameter | Integer32 | NA |
BaseOffset | Used to calculate the address | Integer32 | NA |