Click here to return to the Basic page
The Index Lookup Table block lets you access values stored in a lookup table (LUT).
There is a matrix of values in the table. The size of the table is user determined. There are two inputs, one for the X index and one for the Y index. In the above given example of 3×2 table
To use this block drag it into the workspace and click 'OpenGrid' to open the Table Editor window
Name | ADSP-214xx | ADSP-215xx/SC5xx | ADAU145x/146x |
---|---|---|---|
———————————————— | ——————-- | ——————————-- | —————————- |
Index LookUp Table 2D | B | B | S |
Name | Type | Description |
---|---|---|
———————- | ————-- | ———————- |
IndexX | Control | Input X index value |
IndexY | Control | Input Y index value |
Name | Type | Description |
---|---|---|
———————- | ————-- | ———————- |
Output0 | Control | Table value |
GUI Parameter Name | Default Value | Range | Function Description |
---|---|---|---|
—————————————- | ———————- | —————— | —————————————- |
Index X | 1 | 1 to 15 | Number of rows of the table |
Index Y | 1 | 1 to 15 | Number of columns of the table |
Parameter Name | Description | ADSP-214xx/SC5xx/215xx | ADAU145x/146x |
---|---|---|---|
—————————————- | ——————————————————————————-- | —————————————- | —————————- |
MaxIndex X | Number of Rows | Integer32 | Integer32 |
MaxIndex Y | Number of columns | Integer32 | Integer32 |
TableArray | Table values | Float | FixPoint8d24 |