This shows you the differences between two versions of the page.
Previous revisionNext revision | |||
— | resources:tools-software:sigmastudiov2:modules:basic:dspreadback [04 Feb 2020 11:02] – Added an image Sanjeeva Reddy | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | [[resources/ | ||
+ | ====== DSP Readback | ||
+ | \\ | ||
+ | {{: | ||
+ | ===== Description ===== | ||
+ | The DSP Readback block lets you read values back from the DSP at any point in your schematic design. | ||
+ | The number displayed onscreen is the data value sent back from the DSP considering all the blocks to the left of the Readback block. Every time you click Read, this value will be updated with the latest from the DSP. By displaying the output value from any block, in any format desired, Readback is used chiefly for debugging, and probably will prove very handy. | ||
+ | Values can be read back in either hex or decimal. For the latter, you must specify what format you want the number to be displayed in. Any changes to this format will shift the decimal value of the number displayed. | ||
+ | \\ | ||
+ | ===== Usage ===== | ||
+ | The DSP Readback cell can be configured to read back from the target DSP repeatedly at regular intervals. To enable this mode, right-click the cell and select ReadValue. | ||
+ | \\ | ||
+ | ===== Targets Supported ===== | ||
+ | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | ||
+ | |DSP Readback| Yes | Yes|Yes| Yes| | ||
+ | \\ | ||
+ | ===== Pins ===== | ||
+ | ==== Input ==== | ||
+ | |Input0|Audio|Input Channel 0| | ||
+ | ==== Output ==== | ||
+ | |Output0|Control|Output channel 0| | ||
+ | \\ | ||
+ | ===== Configurable Parameters ===== | ||
+ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
+ | \\ | ||
+ | ===== DSP Parameters ===== | ||
+ | ^Parameter Name^Description^ADSP-214xx/ | ||
+ | |Value|Read back value from the DSP|Float| | ||
+ | \\ |