This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:sigmastudiov2:modules:basic:delay [10 May 2021 17:12] – [Configurable Parameters] Nikhin Shetty | resources:tools-software:sigmastudiov2:modules:basic:delay [10 May 2021 17:13] (current) – [Configurable Parameters] Nikhin Shetty | ||
---|---|---|---|
Line 30: | Line 30: | ||
| CurDelay | 1 | 1 to MaxDelay| Current Daly Value| | | CurDelay | 1 | 1 to MaxDelay| Current Daly Value| | ||
| Memory | DM1 | NA | It allows the user to choose in which memory the delay buffer to be stored ( Not for ADSP-214xx, ADSP-215xx/ | | Memory | DM1 | NA | It allows the user to choose in which memory the delay buffer to be stored ( Not for ADSP-214xx, ADSP-215xx/ | ||
- | |NumChannels|1|20|Numer of input and output channels. Change in this value requires re-compilation| | + | |NumChannels|1|20|Number |
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
^ Parameter Name ^ Description ^ ADSP-214xx/ | ^ Parameter Name ^ Description ^ ADSP-214xx/ |