This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudiov2:modules:basic:delay [10 May 2021 12:10] – [Configurable Parameters] Nikhin Shetty | resources:tools-software:sigmastudiov2:modules:basic:delay [10 May 2021 17:13] (current) – [Configurable Parameters] Nikhin Shetty | ||
---|---|---|---|
Line 25: | Line 25: | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
- | |------------------------------|---------------------------|--------------------------------------------------|----------------------------------------------------------| | + | |------------------------------|---------------------------|---------------------------------------------|----------------------------------------------------------| |
| IsSample | True | True / False | Allows the Max and Cur delay controls either in Samples or milliseconds| | | IsSample | True | True / False | Allows the Max and Cur delay controls either in Samples or milliseconds| | ||
| MaxDelay | 1 | 1 to 1500 (Depends on Size of the Memory available)| This control specifies the maximum delay supported for the current instance in samples (32-bit word). Change in this value requires a re-compilation| | | MaxDelay | 1 | 1 to 1500 (Depends on Size of the Memory available)| This control specifies the maximum delay supported for the current instance in samples (32-bit word). Change in this value requires a re-compilation| | ||
| CurDelay | 1 | 1 to MaxDelay| Current Daly Value| | | CurDelay | 1 | 1 to MaxDelay| Current Daly Value| | ||
- | | Memory | + | | Memory | DM1 | NA | It allows the user to choose in which memory the delay buffer to be stored ( Not for ADSP-214xx, ADSP-215xx/ |
- | |NumChannels|1|20|Numer of input and output channels. Change in this value requires re-compilation| | + | |NumChannels|1|20|Number |
- | \\ | + | |
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
+ | ^ Parameter Name ^ Description ^ ADSP-214xx/ | ||
| ---------------------------------------- | -------------------------------------------------------------------------------- | ---------------------------------------- | ---------------------------- | | | ---------------------------------------- | -------------------------------------------------------------------------------- | ---------------------------------------- | ---------------------------- | | ||
- | |Delay| Current Delay value in bytes. (Cur * 4)|Float|FixPoint8d24 | + | |Delay| Current Delay value in bytes. (Cur * 4)|Integer32|Integer32| |
+ | |MaxDelay| Maximum number of Delay value| Integer32 | NA | | ||
\\ | \\ |