This is an old revision of the document!
Click here to return to the Basic page
The Data Controlled Clip is a hard-clipper that clips the input data signal according to threshold values set by data control input pins.
Name | ADSP-214xx(Sample) | ADSP-214xx(Block) | ADSP-215xx/ADSP-SC5xx(Sample) | ADSP-215xx/ADSP-SC5xx(Block) |
---|---|---|---|---|
Data Controlled Clip | Yes | Yes | Yes | Yes |
High_Threshold | Control | Threshold clip level for the top of the waveform |
Low_Threshold | Control | Threshold clip level for the bottom of the waveform |
Input0 | Audio | Input Channel 0 |
Output0 | Audio | Hard clipped output audio |
GUI Parameter Name | Default Value | Range | Function Description |
---|---|---|---|
NumChannels | 1 | 20 | Number of input and output channels. Change in channels requires re-compilation |
No DSP Parameters