This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:sigmastudiov2:modules:basic:absmaxvaluehold [14 Jan 2021 16:29] – [Absolute Max Value Hold] Nikhin Shetty | resources:tools-software:sigmastudiov2:modules:basic:absmaxvaluehold [13 Sep 2022 11:36] – Updates Images Angu Sewa | ||
---|---|---|---|
Line 2: | Line 2: | ||
====== Absolute Max Value Hold ====== | ====== Absolute Max Value Hold ====== | ||
\\ | \\ | ||
- | {{: | + | {{: |
===== Description ===== | ===== Description ===== | ||
The AbsMaxValueHold block monitors one (or more) input(s) and routes the absolute max value of the input to the output. This block helds the absolute max value while the control input is 1 and reset the absolute max value while the control input is 0. | The AbsMaxValueHold block monitors one (or more) input(s) and routes the absolute max value of the input to the output. This block helds the absolute max value while the control input is 1 and reset the absolute max value while the control input is 0. | ||
\\ | \\ | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
- | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | + | ^ Name ^ ADSP-214xx ^ ADSP-215xx/ |
- | |AbsMaxValueHold| Yes | Yes|Yes| Yes| | + | | ------------------------------------------------------------ |
+ | |AbsMaxValueHold| B/S | B/S | S | | ||
\\ | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | |------------------------------|------------------------------------------------------------|------------------------------| | ||
|Reset|Control|Resets the absolute maximum value| | |Reset|Control|Resets the absolute maximum value| | ||
- | |Input0|Audio|Input channel | + | |Input<fc # |
+ | Note: | ||
+ | * <fc # | ||
==== Output ==== | ==== Output ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
- | |Output0|Audio|Output channel | + | |------------------------------|------------------------------------------------------------|------------------------------| |
+ | |Output | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
+ | |------------------------------|---------------------------|----------------------------|----------------------------------------------------------| | ||
|NumChannels|1| 20|Number of input and output channels. Change in this value requires re-compilation| | |NumChannels|1| 20|Number of input and output channels. Change in this value requires re-compilation| | ||
- | ===== DSP Parameters ===== | ||
- | No DSP parameters | ||