This is an old revision of the document!
Click here to return to the Arithmetic and Logic page
The Signal Subtract block subtracts the input signals(all input signals are subtracted to the first signal) and outputs the difference result.
Name | ADSP-214xx(Sample) | ADSP-214xx(Block) | ADSP-215xx/ADSP-SC5xx(Sample) | ADSP-215xx/ADSP-SC5xx(Block) |
---|---|---|---|---|
Signal Subtract | Yes | Yes | Yes | Yes |
Name | Type | Description |
---|---|---|
Input0 | Audio | Input channel 0 |
Input1 | Audio | Input channel 1 |
Name | Type | Description |
---|---|---|
Difference | Audio | Result of the difference of first channel and sum of other channels |
GUI Parameter Name | Default Value | Range | Function Description |
---|---|---|---|
NumChannels | 2 | 20 | Number of input channels. Change in this value requires re-compilation |
No DSP parameters