This is an old revision of the document!
Click here to return to the Arithmetic and Logic page
The Signal Divide block divide two incoming signals. The division is performed by using the Newton-Rapson method.
Name | ADSP-214xx(Sample) | ADSP-214xx(Block) | ADSP-215xx/ADSP-SC5xx(Sample) | ADSP-215xx/ADSP-SC5xx(Block) |
---|---|---|---|---|
Signal Divide | Yes | Yes | Yes | Yes |
Name | Type | Description |
---|---|---|
Divident | Control | Input channel 0 |
Divisor | Control | Input channel 1 |
Result | Control | Output channel 0 |
No configurable parameters
NO DSP Parameters