This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudiov2:modules:arithmeticandlogic:runningaverage [04 Jun 2020 13:11] – [DSP Parameters] Krithika Manchale | resources:tools-software:sigmastudiov2:modules:arithmeticandlogic:runningaverage [07 May 2021 07:09] (current) – [Output] Krithika Manchale | ||
---|---|---|---|
Line 7: | Line 7: | ||
\\ | \\ | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
- | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | + | ^ Name |
- | |Running Average | + | | ------------------------------ |
+ | | Running Avg| B | ||
\\ | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | ------------------------------------ | ------------------------------ | ---------------------------------------- | | ||
|Input0|Audio|Input channel 0| | |Input0|Audio|Input channel 0| | ||
==== Output ==== | ==== Output ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | ------------------------------------ | ------------------------------ | ---------------------------------------- | | ||
|Output0|Audio|Output channel 0| | |Output0|Audio|Output channel 0| | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
- | ^GUI Parameter Name^Default Value^Range^Function Description^ | + | ^GUI Parameter Name ^ Default Value |
+ | | ------------------------------ | ||
|MaxBlockSizeSet|1|1 -1500 (Depends on the size of memory available)|Specifies the maximum samples for averaging. Change in this value requires a re-compilation| | |MaxBlockSizeSet|1|1 -1500 (Depends on the size of memory available)|Specifies the maximum samples for averaging. Change in this value requires a re-compilation| | ||
|CurrentBlockSize|1|1 - MaxBlockSizeSet| Number of samples to be averaged. Change in this value requires a re-compilation| | |CurrentBlockSize|1|1 - MaxBlockSizeSet| Number of samples to be averaged. Change in this value requires a re-compilation| | ||
Line 26: | Line 30: | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
- | ^Parameter Name^Description^ADSP-214xx/ | + | ^Parameter Name^ Description^ |
- | |MaxBlockSizeSet|Specifies the maximum samples for averaging|Float| | + | | ------------------------------------ |
- | |MaxCurrentBlockSize|Number of samples to be averaged|Float| | + | |MaxBlockSizeSet |
- | |OneOverN|Inverse of CurrentBlockSize|Float| | + | |MaxCurrentBlockSize |
+ | |OneOverN| Inverse of CurrentBlockSize|Float| | ||
===== DSP Parameter Computation ===== | ===== DSP Parameter Computation ===== | ||
NA | NA |