This is an old revision of the document!
Click here to return to the Arithmetic and Logic page
The RMSWithTC block computes the RMS of the input signals with time constant specified in the text field.
Name | ADSP-214xx | ADSP-215xx/SC5xx | ADAU145x/146x |
---|---|---|---|
—————————— | ——————-- | ——————————-- | —————————- |
RMSWithTC | S/B | S/B | NA |
Name | Type | Description |
---|---|---|
—————————— | ——————-- | ——————————-- |
Input0 | Audio | Input channel 10 |
Name | Type | Description |
---|---|---|
—————————— | ——————-- | ——————————-- |
Output0 | Audio | Output channel 0 |
GUI Parameter Name | Default Value | Range | Function Description |
---|---|---|---|
—————————————- | —————————- | ————————————- | ———————————— |
TimeConstant | 121 | 1-8686 | Determines how rapidly the RMS value is to be computed with any change in the input level |
IsDBps | False | True/False | Control value in dB/s or ms |
NumChannels | 2 | 20 | Number of input and Output channels. Change in this value requires re-compilation |
Parameter Name | Description | ADSP-214xx/215xx/SC5xx |
---|---|---|
——————————-- | ———————————————- | ——————————————- |
TimeConstant | TC for RMS value with change in input | Float |
TimeConstant = ABS(1-10^(TimeConstant(linear)/(10*FS))) Where FS is the Sampling rate