Wiki

This version is outdated by a newer approved version.DiffThis version (14 Jan 2021 12:31) is a draft.
Approvals: 0/1

This is an old revision of the document!


Click here to return to the Arithmetic and Logic page

One Shot Rise



Description

The One Shot Rise block outputs a trigger signal based upon the rising edge of the input signal. At the first non-zero rising edge of the input signal, the output signal will go high and remain high.For One Shot Raise Reset block the output signal will remain high until a non-zero input signal is seen on the rest pin. The reset pin clears the output back to zero and will maintain the output at zero while the signal on the reset pin is non-zero.

If the input signal starts high, the output signal will start and remain high.

Variants

  1. OneShotRise
  2. OneShotRiseReset


Targets Supported

NameADSP-214xx(Sample)ADSP-214xx(Block)ADSP-215xx/ADSP-SC5xx(Sample)ADSP-215xx/ADSP-SC5xx(Block)
OneShotRise Yes YesYes Yes
OneShotRiseReset Yes YesYes Yes


Pins

Input

NameTypeDescription
InputAudioInput signal that is monitored for the first falling edge
ResetControlResets the output trigger signal back to zero(only for OneShotRiseReset)

Output

NameTypeDescription
OutputControlSets bit position of the output “1” flag


Configurable Parameters

GUI Parameter NameDefault ValueRangeFunction Description
Selected BitBit:0Bit:30Sets bit position of Output'1' Flag.


DSP Parameters

Parameter NameDescriptionADSP-214xx/215xx/SC5xx
BitVal Compute & set the bit position value FixInt32


resources/tools-software/sigmastudiov2/modules/arithmeticandlogic/oneshotraise.1610623913.txt.gz · Last modified: 14 Jan 2021 12:31 by Nikhin Shetty