This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:tools-software:sigmastudiov2:modules:arithmeticandlogic:oneshotraise [06 May 2021 14:33] – [DSP Parameters] Krithika Manchale | resources:tools-software:sigmastudiov2:modules:arithmeticandlogic:oneshotraise [07 May 2021 07:48] – [DSP Parameters] Krithika Manchale | ||
---|---|---|---|
Line 24: | Line 24: | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
- | | --------------------------------------- | ---------------------------- | --------------------------------------- | | + | | --------------------------------------- | ---------------------------- | ------------------------------------------------------- | |
|Input|Audio|Input signal that is monitored for the first falling edge| | |Input|Audio|Input signal that is monitored for the first falling edge| | ||
|Reset|Control|Resets the output trigger signal back to zero(only for OneShotRiseReset)| | |Reset|Control|Resets the output trigger signal back to zero(only for OneShotRiseReset)| | ||
==== Output ==== | ==== Output ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
- | | --------------------------------------- | ---------------------------- | --------------------------------------- | | + | | --------------------------------------- | ---------------------------- | -------------------------------------------------------- | |
|Output|Control|Sets bit position of the output “1” flag| | |Output|Control|Sets bit position of the output “1” flag| | ||
\\ | \\ | ||
Line 38: | Line 38: | ||
\\ | \\ | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
- | ^Parameter Name^Description^ADSP-214xx/ | + | ^Parameter Name^Description^ADSP-214xx/ |
- | | ------------------------------------ | -------------------------------------------------------------------------- | + | | ------------------------------------ | ----------------------------------------------------------------- | ---------------------------------------- | --------------------------------------- | |
|BitVal| Compute & set the bit position value| FixInt32| FixInt32| | |BitVal| Compute & set the bit position value| FixInt32| FixInt32| | ||
\\ | \\ | ||