This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:tools-software:sigmastudiov2:modules:arithmeticandlogic:absolutevalue [31 Oct 2019 10:33] – created Sanjeeva Reddy | resources:tools-software:sigmastudiov2:modules:arithmeticandlogic:absolutevalue [14 Sep 2022 13:38] (current) – [Output] Angu Sewa | ||
---|---|---|---|
Line 1: | Line 1: | ||
[[resources/ | [[resources/ | ||
====== Absolute Value ====== | ====== Absolute Value ====== | ||
+ | \\ | ||
+ | {{: | ||
===== Description ===== | ===== Description ===== | ||
The Absolute Value block coverts all negative components of the input to positive components. | The Absolute Value block coverts all negative components of the input to positive components. | ||
- | + | \\ | |
===== Targets Supported ===== | ===== Targets Supported ===== | ||
- | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | + | ^ Name |
- | |Absolute Value | Yes | Yes|Yes| Yes| | + | | ------------------------------ | -------------------- | -------------------------------- | ---------------------------- | |
+ | | Absolute Value | ||
+ | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
- | |Input0|Audio|Input channel | + | | ------------------------------------ | ------------------------------ | ---------------------------------------- | |
+ | |Input|Audio|Input channel| | ||
==== Output ==== | ==== Output ==== | ||
- | |Output0|Control|Output channel 0| | + | ^Name^Type^Description^ |
+ | | ------------------------------------ | ------------------------------ | ---------------------------------------- | | ||
+ | |Output|Control|Output channel 0| | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== |