This is an old revision of the document!
Click here to return to the Arithmetic and Logic page
The AB In-CD Out Condition block lets you compare the sample-by-sample level of two incoming signals (A & B) and output the sample of one of two new signals (C & D), depending on the condition.
This algorithm works only for DSP's with conditional instruction.
Click the icon in the block to select the condition you want to check:
When the condition is true, output sample is C; otherwise, it's D.
Name | ADSP-214xx(Sample) | ADSP-214xx(Block) | ADSP-215xx/ADSP-SC5xx(Sample) | ADSP-215xx/ADSP-SC5xx(Block) |
---|---|---|---|---|
ABInCDOutCondition | Yes | Yes | Yes | Yes |
Name | Type | Description |
---|---|---|
Input0 | Audio | Input channel 0 (Input Signal A) |
Input1 | Audio | Input channel 1 (Input Signal B) |
Input2 | Audio | Input channel 0 (Input Signal C) |
Input3 | Audio | Input channel 1 (Input Signal D) |
Output | Audio | Output channel |
No configurable parameter
NO DSP parameters