This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudiov2:modules:advanceddsp:downsampling [14 Jan 2021 11:01] – [Down Sampling] Nikhin Shetty | resources:tools-software:sigmastudiov2:modules:advanceddsp:downsampling [12 May 2021 13:21] (current) – John Joseph | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | [[resources/ | + | [[resources/ |
====== Down Sampling ====== | ====== Down Sampling ====== | ||
Line 9: | Line 9: | ||
\\ | \\ | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
- | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | + | ^ Name ^ ADSP-214xx ^ ADSP-215xx/ |
- | |DownSampler| No | No|No| Yes| | + | | ------------------------------ |
+ | | Down-Sampler | ||
\\ | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | ---------------------- | -------------- | ---------------------- | | ||
|Input|Audio|Input channel| | |Input|Audio|Input channel| | ||
==== Output ==== | ==== Output ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | ---------------------- | -------------- | ---------------------- | | ||
|Output|Audio|Down sampled output| | |Output|Audio|Down sampled output| | ||
\\ | \\ | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
+ | ==== ADSP-214xx/ | ||
^GUI Parameter Name^Default^Range^Function Description^ | ^GUI Parameter Name^Default^Range^Function Description^ | ||
+ | | ---------------------------------------- | ---------------------- | ------------------ | ---------------------------------------- | | ||
|Factor|2|2, | |Factor|2|2, | ||
|AntiAliasFilter|False|True/ | |AntiAliasFilter|False|True/ | ||
+ | \\ | ||
+ | ==== ADAU145x/ | ||
+ | ^GUI Parameter Name^Default^Range^Function Description^ | ||
+ | | ---------------------------------------- | ---------------------- | ------------------ | ---------------------------------------- | | ||
+ | |NumChannels|1|1-20|Number of channels| | ||
+ | |Factor|2|2, | ||
\\ | \\ | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
- | ^Name^Description^ADSP-214xx/ | + | ^Name^Description^ADSP-214xx/ |
- | |Factor |The factor at with the input sample rate will be divided|Float| | + | | --------------------------- | ---------------------------------------------------------------------------------- | ---------------------------------------- | -------------------------- | |
- | |NFilterTaps |Number of antialiasing filter coefficients|Float| | + | |Factor |The factor at with the input sample rate will be divided|Float|FixedPoint8d24| |
- | |FIRCoeffs |coefficients|Float| | + | |NFilterTaps |Number of antialiasing filter coefficients|Float|NA| |
+ | |FIRCoeffs |coefficients|Float|NA| | ||
\\ | \\ | ||
- | ===== DSP Parameter Computation ===== | + | |
- | NFilterTaps | + | |