This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:sigmastudiov2:modules:adialgorithms:superbass [04 Feb 2020 06:05] – Added an image Sanjeeva Reddy | resources:tools-software:sigmastudiov2:modules:adialgorithms:superbass [21 Sep 2022 07:56] – Updates super bass mono image Ashwin PS | ||
---|---|---|---|
Line 1: | Line 1: | ||
[[resources/ | [[resources/ | ||
====== SuperBass ====== | ====== SuperBass ====== | ||
- | \\ | + | {{: |
- | {{: | + | {{: |
===== Description ===== | ===== Description ===== | ||
\\ | \\ | ||
- | The Superbass | + | The Super Bass block is a bass enhancement algorithm specifically designed to compensate for the poor low end response of small speakers by using psychoacoustic principles to improve the perceived bass response. |
\\ | \\ | ||
===== Variants ===== | ===== Variants ===== | ||
- | - SuperBass | + | - Super Bass (Mono) |
- | - SuperBass | + | - Super Bass (Stereo) |
\\ | \\ | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
- | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | + | ^ Name ^ ADSP-214xx ^ ADSP-215xx/ |
- | |SuperBass Mono| No | Yes|No| Yes| | + | | ------------------------------ |
- | |SuperBass | + | | Super Bass (Mono) | B | B | S |
+ | | Super Bass (Stereo) | B | ||
\\ | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | ---------------------- | -------------- | ---------------------- | | ||
|Input0|Audio|Input channel0| | |Input0|Audio|Input channel0| | ||
|Input1|Audio|Input Channel1 (only for stereo)| | |Input1|Audio|Input Channel1 (only for stereo)| | ||
==== Output ==== | ==== Output ==== | ||
+ | ^Name^Type^Description^ | ||
+ | | ---------------------- | -------------- | ---------------------- | | ||
|Output0|Audio|Output channel0| | |Output0|Audio|Output channel0| | ||
|Output1|Audio|Output channel1 (only for stereo)| | |Output1|Audio|Output channel1 (only for stereo)| | ||
Line 27: | Line 31: | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
- | |Intensity| 1.3 | 0.1 to 3 | Controls how much gain applied to the artificially generated higher harmonics(Above cross over frequency).| | + | | ---------------------------------------- | ---------------------- | ------------------ | ---------------------------------------- | |
+ | |Intensity| 1.3 | 0.1 to 3 | Controls how much gain is applied to the artificially generated higher harmonics(Above cross over frequency).| | ||
|BassGain| 1.2 | 0.1 to 3|Controls the gain applied to the input signal below the cross over frequency| | |BassGain| 1.2 | 0.1 to 3|Controls the gain applied to the input signal below the cross over frequency| | ||
|XOverFrequency| 90 Hz| 20 to 500 Hz| The signals below this frequency are considered to be in the bass range. These signals will be used for the bass enhancement algorithm. Higher harmonics of these signals will be generated above the crossover frequency, giving the impression of increased bass. | | |XOverFrequency| 90 Hz| 20 to 500 Hz| The signals below this frequency are considered to be in the bass range. These signals will be used for the bass enhancement algorithm. Higher harmonics of these signals will be generated above the crossover frequency, giving the impression of increased bass. | | ||
Line 33: | Line 38: | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
- | ^Parameter Name^Description^ADSP-214xx/ | + | ^ Parameter Name |
- | |RMS|RMS time constant for the detector to respond to the change in input signal level |Float| | + | | ---------------------------------------- | -------------------------------------------------------------------------------- | ---------------------------------------- | ---------------------------- | |
- | |BassGain|Gain applied to the input signal below the cross over frequency|Float| | + | |RMS|RMS time constant for the detector to respond to the change in input signal level |Float|8.24 Format| |
- | |Intensity|Gain applied to the artificially generated higher harmonics(Above cross over frequency)|Flaot| | + | |BassGain|Gain applied to the input signal below the cross over frequency|Float|8.24 Format| |
- | |Bypass_ON|Enabled/ | + | |Intensity|Gain applied to the artificially generated higher harmonics(Above cross over frequency)|Flaot|8.24 Format| |
+ | |Bypass_ON|Enabled/ |