This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:sigmastudiov2:modules:adialgorithms:dynamicbassboost [21 Sep 2022 19:45] – Updates Dynamic bass boost mono and stereo images Ashwin PS | resources:tools-software:sigmastudiov2:modules:adialgorithms:dynamicbassboost [14 Mar 2024 13:42] (current) – Formatting corrected John Joseph | ||
---|---|---|---|
Line 1: | Line 1: | ||
[[resources/ | [[resources/ | ||
====== Dynamic Bass Boost ====== | ====== Dynamic Bass Boost ====== | ||
- | === Dynamic Bass Boost Mono === | ||
{{: | {{: | ||
- | === Dynamic Bass Boost Stereo === | + | \\ |
- | {{: | + | |
===== Description ===== | ===== Description ===== | ||
\\ | \\ | ||
Line 10: | Line 8: | ||
The filter calculates its bass boost between the Threshold and minimum Gain settings. A fixed maximum bass is applied to inputs above the minimum gain and below the Threshold level. | The filter calculates its bass boost between the Threshold and minimum Gain settings. A fixed maximum bass is applied to inputs above the minimum gain and below the Threshold level. | ||
+ | \\ | ||
\\ | \\ | ||
===== Variants ===== | ===== Variants ===== | ||
Line 15: | Line 14: | ||
- Dynamic Bass Boost Stereo | - Dynamic Bass Boost Stereo | ||
\\ | \\ | ||
- | |||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
^ Name ^ ADSP-214xx ^ ADSP-215xx/ | ^ Name ^ ADSP-214xx ^ ADSP-215xx/ | ||
- | | ---------------------------------------- | -------------------- | -------------------------------- | ---------------------------- | | + | | Dynamic Bass Boost Mono | Block and Sample |
- | | Dynamic Bass Boost Mono | B/S | + | | Dynamic Bass Boost Stereo| |
- | | Dynamic Bass Boost Stereo| | + | |
\\ | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
- | | ---------------------- | -------------- | ---------------------- | | ||
|Input0|Audio|Input channel0| | |Input0|Audio|Input channel0| | ||
|Input1|Audio|Input Channel1 (only for stereo)| | |Input1|Audio|Input Channel1 (only for stereo)| | ||
==== Output ==== | ==== Output ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
- | | ---------------------- | -------------- | ---------------------- | | ||
|Output0|Audio|Output channel0| | |Output0|Audio|Output channel0| | ||
|Output1|Audio|Output channel1 (only for stereo)| | |Output1|Audio|Output channel1 (only for stereo)| | ||
+ | \\ | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
- | | ---------------------------------------- | ---------------------- | ------------------ | ---------------------------------------- | | ||
|LowPassFrequency|250 Hz| 20 to 250 Hz| Frequencies below the LowPassFrequency settings are used by the detector to determine the boost amount| | |LowPassFrequency|250 Hz| 20 to 250 Hz| Frequencies below the LowPassFrequency settings are used by the detector to determine the boost amount| | ||
|HighThreshold| -5 dB| -45 to 10 dB| Higher Threshold of the detector.Any signal coming into the detector above the threshold level wil not influence the boost calculation. it recieves a fixed boost| | |HighThreshold| -5 dB| -45 to 10 dB| Higher Threshold of the detector.Any signal coming into the detector above the threshold level wil not influence the boost calculation. it recieves a fixed boost| | ||
Line 43: | Line 38: | ||
|BoostFrequency|6 Hz| 0 to 16 Hz|Controls the maximum gain applied to the algorithm| | |BoostFrequency|6 Hz| 0 to 16 Hz|Controls the maximum gain applied to the algorithm| | ||
|BassFrequency|60 hz|20 to 300 Hz|Cut off frequency for the boosting filter| | |BassFrequency|60 hz|20 to 300 Hz|Cut off frequency for the boosting filter| | ||
+ | \\ | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
^ Parameter Name ^ Description ^ ADSP-214xx/ | ^ Parameter Name ^ Description ^ ADSP-214xx/ | ||
- | | ---------------------------------------- | -------------------------------------------------------------------------------- | ---------------------------------------- | ---------------------------- | | ||
|TimeConstant|Rms time constant for the detector for change in input signal level|Float|8.24 Format| | |TimeConstant|Rms time constant for the detector for change in input signal level|Float|8.24 Format| | ||
|BassFrequency|Cut off frequency for the boosting filter|Float|8.24 Format| | |BassFrequency|Cut off frequency for the boosting filter|Float|8.24 Format| | ||