This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudiov2:modules:adialgorithms:autoeq [21 Sep 2022 09:43] – Updates auto eq image Ashwin PS | resources:tools-software:sigmastudiov2:modules:adialgorithms:autoeq [14 Mar 2024 13:29] (current) – Formatting corrected John Joseph | ||
---|---|---|---|
Line 1: | Line 1: | ||
[[resources/ | [[resources/ | ||
====== Automatic Speaker EQ ====== | ====== Automatic Speaker EQ ====== | ||
- | {{: | + | {{: |
- | + | ||
- | ===== Description ===== | + | |
\\ | \\ | ||
+ | ===== Description ===== | ||
The Automatic Speaker EQ algorithm is aimed at reducing the design time of speaker systems by automatically tuning filters to create the desired frequency response of the speaker. The algorithm is capable of tuning one, two, and three way systems. | The Automatic Speaker EQ algorithm is aimed at reducing the design time of speaker systems by automatically tuning filters to create the desired frequency response of the speaker. The algorithm is capable of tuning one, two, and three way systems. | ||
+ | \\ | ||
\\ | \\ | ||
===== Variants ===== | ===== Variants ===== | ||
Line 12: | Line 12: | ||
- Three Way Auto EQ | - Three Way Auto EQ | ||
\\ | \\ | ||
- | |||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
^ Name ^ ADSP-214xx ^ ADSP-215xx/ | ^ Name ^ ADSP-214xx ^ ADSP-215xx/ | ||
- | | ---------------------------------- | -------------------- | -------------------------------- | ---------------------------- | | ||
| Single Band Auto EQ | B | B | S | | | Single Band Auto EQ | B | B | S | | ||
| Two Way Auto EQ | B | B | S | | | Two Way Auto EQ | B | B | S | | ||
Line 23: | Line 21: | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
- | | ---------------------- | -------------- | ---------------------- | | ||
|Input0|Audio|Input| | |Input0|Audio|Input| | ||
+ | \\ | ||
==== Output ==== | ==== Output ==== | ||
===Single Band Auto EQ=== | ===Single Band Auto EQ=== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
- | | ---------------------- | -------------- | ---------------------- | | ||
|Driver|Audio|Equalized output| | |Driver|Audio|Equalized output| | ||
+ | \\ | ||
===Two Way Auto EQ=== | ===Two Way Auto EQ=== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
- | | ---------------------- | -------------- | ---------------------- | | ||
|Woofer|Audio|Equalized Woofer Channel| | |Woofer|Audio|Equalized Woofer Channel| | ||
|Tweeter|Audio|Equalized Tweeter Channel| | |Tweeter|Audio|Equalized Tweeter Channel| | ||
+ | \\ | ||
===Three Way Auto EQ=== | ===Three Way Auto EQ=== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
- | | ---------------------- | -------------- | ---------------------- | | ||
|Woofer|Audio|Equalized Woofer Channel| | |Woofer|Audio|Equalized Woofer Channel| | ||
|Mid|Audio|Equalized Mid Driver Channel| | |Mid|Audio|Equalized Mid Driver Channel| | ||
|Tweeter|Audio|Equalized Tweeter Channel| | |Tweeter|Audio|Equalized Tweeter Channel| | ||
+ | \\ | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
- | |||
=====Source Tab===== | =====Source Tab===== | ||
When first opening the control, the source tab will be visible. This is where the response(s) of the desired speakers are loaded. Compatible formats include Impulse Responses with one measurement per line and Frequency responses in the MLSSA file format. | When first opening the control, the source tab will be visible. This is where the response(s) of the desired speakers are loaded. Compatible formats include Impulse Responses with one measurement per line and Frequency responses in the MLSSA file format. |