Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:tools-software:sigmastudiov2:gettingstarted:flash_the_loader_file [13 Feb 2023 13:22] – note added John Joseph | resources:tools-software:sigmastudiov2:gettingstarted:flash_the_loader_file [13 Feb 2023 14:03] – John Joseph |
---|
Batch files for programming the flash are provided under '**SigmaStudioPlus-Relx.y.z\Target\Utilities\FlashProgrammer**' folder and pre-built loader files (LDR) are provided under '**SigmaStudioPlus-Relx.y.z\Target\Examples\LDR**' folder. | Batch files for programming the flash are provided under '**SigmaStudioPlus-Relx.y.z\Target\Utilities\FlashProgrammer**' folder and pre-built loader files (LDR) are provided under '**SigmaStudioPlus-Relx.y.z\Target\Examples\LDR**' folder. |
\\ | \\ |
<note>The path of cldp.exe inside the batch files should be updated based on the CCES version number and path of installation. The batch file by default will have the CCESS version recommended for the given release and the default installation path</note> | <note>The path of cldp.exe inside the batch files should be updated based on the CCES version number and path of installation. The batch file by default will have the CCES version recommended for the given release and the default installation path</note> |
\\ | \\ |
Use the following command to program the flash on ADSP-SC584 EZ-Board using the pre-built SS_App_SC584.ldr loader file. | Use the following command to program the flash on ADSP-SC584 EZ-Board using the pre-built SS_App_SC584.ldr loader file. |