The following are the list of hardware components required for setting up the demo application.
The SigmaStudio+ demonstration setup for ADAU145x and ADAU146x includes a Host PC running SigmaStudio+ which is connected to the evaluation board. The connection is achieved using a USB-to-SPI converter. The EVAL-ADUSB2EBZ or Aardvark I2C/SPI acts as the USB-to-SPI converter, which is connected to the PC through a USB port and to the evaluation board through SPI pins.
The EVAL-ADUSB2EBZ (hereafter referred to as the ‘USBi’) has a 10 pin socket. This is connected to SPI CONTROL PORT/CONTROL PORT header on the board.
Connect Aardvark I2C/SPI Host Adapter to the PC running SigmaStudio using a USB cable. Aardvark I2C/SPI Host Adapter has a 10 pin socket. This is connected to SPI CONTROL PORT/CONTROL PORT header on the board.
Connect an analog audio source and headphones/speakers to the audio ports on the EVAL board.
Connect the power and reset the board by pressing the ‘RESET’ button on the EVAL Board.