This is an old revision of the document!
Use the sequence window to define a custom sequence of data read/write operations between SigmaStudio and a target hardware device connected via USB. Commands can be dragged from the capture window or created manually. Sequences are independent of the SigmaStudio+ project file and can be saved and recalled to files.
The Sequence window is docked at the bottom by default. The option to add sequences from capture window is available. Also there is an option to define the operation manually. A separate packet can be created, specifying he address of the location where the data packet is to be written along with the protocol to be used, which is usually SPI or I2C. Finally when the sequence is ready, pressing the download button on the sequence window, will send the packet to the target.