This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:sigmastudio [17 Aug 2016 17:08] – [Feature Wishlist] Benoit BOUCHEZ | resources:tools-software:sigmastudio [29 Apr 2020 21:54] – Changed feature request link Joshua Berlin | ||
---|---|---|---|
Line 9: | Line 9: | ||
This tool was originally tailored for engineers tasked with migrating analog sound processing systems to digital ones; yet it is powerful enough to satisfy more experienced DSP designers. SigmaStudio can help users reduce development times, lower costs without sacrificing quality or performance. | This tool was originally tailored for engineers tasked with migrating analog sound processing systems to digital ones; yet it is powerful enough to satisfy more experienced DSP designers. SigmaStudio can help users reduce development times, lower costs without sacrificing quality or performance. | ||
- | * See [[resources/ | + | * See [[resources/ |
* To get started, follow the [[resources/ | * To get started, follow the [[resources/ | ||
* To see what SigmaStudio can do, check out the [[resources/ | * To see what SigmaStudio can do, check out the [[resources/ | ||
- | <WRAP important> | ||
- | |||
- | <WRAP important> | ||
<WRAP download> | <WRAP download> | ||
- | |||
- | <WRAP important> | ||
- | |||
- | ---- | ||
===== Documentation Sections ===== | ===== Documentation Sections ===== | ||
Line 33: | Line 26: | ||
[[resources/ | [[resources/ | ||
\\ This section describes the basic functions of the SigmaStudio software. | \\ This section describes the basic functions of the SigmaStudio software. | ||
+ | |||
+ | [[resources/ | ||
+ | \\ This section describes the list of ICs supported by SigmaStudio. | ||
[[resources/ | [[resources/ | ||
Line 46: | Line 42: | ||
\\ This section contains tutorials and guides to help users understand and use SigmaStudio. | \\ This section contains tutorials and guides to help users understand and use SigmaStudio. | ||
+ | [[resources/ | ||
+ | \\ This section contains features added and bugs fixed in each of the releases. | ||
---- | ---- | ||
Line 60: | Line 58: | ||
===== Feature Wishlist ===== | ===== Feature Wishlist ===== | ||
- | [[resources/tools-software/sigmastudio/ | + | Please submit feature requests for SigmaStudio in the [[ez> |
- | + | ||
- | **Bitwise logic support for ADAU170x chip** | + | |
- | * Description : SigmaStudio only includes " | + | |
- | * Notes : N/A | + | |
- | * Developer feedback : | + | |
- | **Zero phase on VCO ON/OFF command ** | ||
- | * Description : when a VCO is turned OFF, it is simply a switch forcing the output signal to 0. The oscillator keeps running and when the VCO is turned ON, the sinus signal phase is completely random. The zero phase feature should allow the sinus phase to be reset when the switch goes from OFF to ON | ||
- | * Notes : N/A | ||
- | * Developer feedback : |