This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudio:usingsigmastudio:tcpipchannels [11 Nov 2016 05:54] – Suhasini Raghuram | resources:tools-software:sigmastudio:usingsigmastudio:tcpipchannels [26 Jun 2019 12:08] (current) – TCPIP Added for ADAU146x Sanjeeva Reddy | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ======TCP/ | + | ======TCP/ |
[[resources/ | [[resources/ | ||
\\ | \\ | ||
- | |||
The TCP/IP channel can be used to connect with the SigmaDSP in case the SigmaDSP is present at a different location and cannot be physically connected the the PC that is running SigmaStudio. | The TCP/IP channel can be used to connect with the SigmaDSP in case the SigmaDSP is present at a different location and cannot be physically connected the the PC that is running SigmaStudio. | ||
Line 9: | Line 8: | ||
The TCPIP channel is present under the Communication Channels tree as shown in the figure below: | The TCPIP channel is present under the Communication Channels tree as shown in the figure below: | ||
- | {{ : | + | {{ : |
Drag and Drop the channel onto the configuration tab and connect it to the IC. | Drag and Drop the channel onto the configuration tab and connect it to the IC. | ||
Line 36: | Line 35: | ||
|Block / safeload write bit| This field indicates whether the write packet is a block write or a safeload write| | |Block / safeload write bit| This field indicates whether the write packet is a block write or a safeload write| | ||
|Channel number| This indicates the channel number| | |Channel number| This indicates the channel number| | ||
+ | |Total length| This indicates the total length of the write packet. It is 4 bytes long| | ||
+ | |Chip address| This is the address of the chip to which the data has to be written| | ||
+ | |Data Length| This is the length of the data. This is 4 bytes long| | ||
+ | |Address| This is the address of the module whose data is being written to the DSP. This is 2 bytes long| | ||
+ | |Data| This is the data to be written| | ||
===== Readback from the DSP ===== | ===== Readback from the DSP ===== | ||
+ | In order to achieve readback, SigmaStudio send a read request. The server connected to SigmaDSP must respond to the read request with a read response. | ||
- | SigmaStudio sends a read request packet to the SigmaDSP. | + | ==== Read Request format ==== |
+ | The read request format is as shown | ||
{{ : | {{ : | ||
+ | ===Fields === | ||
+ | ^Field^Description^ | ||
+ | |Control| This is the control bit that is used to indicate that it is a read packet. Its value is 0x0A | | ||
+ | |Total length| This indicates the total length of the read packet. It is 4 bytes long| | ||
+ | |Chip address| This is the address of the chip for which the data has to be read from| | ||
+ | |Data Length| This is the length of the data to read. This is 4 bytes long| | ||
+ | |Address| This is the address of the module whose data is being read from the DSP. This is 2 bytes long| | ||
+ | |Reserved| There are two fields reserved for future use.| | ||
+ | |||
+ | |||
+ | ==== Read Response Format ==== | ||
The server connected to SigmaDSP has to respond to the read request in the following format: | The server connected to SigmaDSP has to respond to the read request in the following format: | ||
{{ : | {{ : | ||
+ | |||
+ | \\ | ||
+ | ===Fields === | ||
+ | ^Field^Description^ | ||
+ | |Control| This is the control bit that is used to indicate that it is a read response packet. Its value is 0x0B | | ||
+ | |Total length| This indicates the total length of the read response packet. It is 4 bytes long| | ||
+ | |Chip address| This is the address of the chip to which the data has been read from| | ||
+ | |Data Length| This is the length of the data. This is 4 bytes long| | ||
+ | |Address| This is the address of the module whose data has been read from the DSP. This is 2 bytes long| | ||
+ | |Success / Failure| This byte indicates whether the read operation was a success or failure. It should be populated with a 0 for success and 1 for failure| | ||
+ | |Reserved| This field is reserved for future use| | ||
+ | |Data| This is the data read from the address| |