Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:tools-software:sigmastudio:usingsigmastudio:tcpipchannels [05 Jan 2017 15:36] – [Read Response Format] Ivan Johansenresources:tools-software:sigmastudio:usingsigmastudio:tcpipchannels [26 Jun 2019 12:08] (current) – TCPIP Added for ADAU146x Sanjeeva Reddy
Line 1: Line 1:
-======TCP/IP Channels (ADAU144x / ADAU145x) ======+======TCP/IP Channels (ADAU144x / ADAU145x / ADAU146x) ======
  
 [[resources/tools-software/sigmastudio/usingsigmastudio|Click here to return to the Using SigmaStudio page]]\\ [[resources/tools-software/sigmastudio/usingsigmastudio|Click here to return to the Using SigmaStudio page]]\\
 \\ \\
- 
  
 The TCP/IP channel can be used to connect with the SigmaDSP in case the SigmaDSP is present at a different location and cannot be physically connected the the PC that is running SigmaStudio. The TCP/IP channel can be used to connect with the SigmaDSP in case the SigmaDSP is present at a different location and cannot be physically connected the the PC that is running SigmaStudio.
Line 9: Line 8:
  
 The TCPIP channel is present under the Communication Channels tree as shown in the figure below: The TCPIP channel is present under the Communication Channels tree as shown in the figure below:
-{{ :resources:tools-software:sigmastudio:usingsigmastudio:channel.jpg?nolink |}}+{{ :resources:tools-software:sigmastudio:usingsigmastudio:tcpip_146x_support.png?nolink |}}
  
 Drag and Drop the channel onto the configuration tab and connect it to the IC.  Drag and Drop the channel onto the configuration tab and connect it to the IC. 
resources/tools-software/sigmastudio/usingsigmastudio/tcpipchannels.txt · Last modified: 26 Jun 2019 12:08 by Sanjeeva Reddy