This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudio:usingsigmastudio:tcpipchannels [05 Jan 2017 15:34] – [Read Request format] Ivan Johansen | resources:tools-software:sigmastudio:usingsigmastudio:tcpipchannels [26 Jun 2019 12:08] (current) – TCPIP Added for ADAU146x Sanjeeva Reddy | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ======TCP/ | + | ======TCP/ |
[[resources/ | [[resources/ | ||
\\ | \\ | ||
- | |||
The TCP/IP channel can be used to connect with the SigmaDSP in case the SigmaDSP is present at a different location and cannot be physically connected the the PC that is running SigmaStudio. | The TCP/IP channel can be used to connect with the SigmaDSP in case the SigmaDSP is present at a different location and cannot be physically connected the the PC that is running SigmaStudio. | ||
Line 9: | Line 8: | ||
The TCPIP channel is present under the Communication Channels tree as shown in the figure below: | The TCPIP channel is present under the Communication Channels tree as shown in the figure below: | ||
- | {{ : | + | {{ : |
Drag and Drop the channel onto the configuration tab and connect it to the IC. | Drag and Drop the channel onto the configuration tab and connect it to the IC. | ||
Line 68: | Line 67: | ||
===Fields === | ===Fields === | ||
^Field^Description^ | ^Field^Description^ | ||
- | |Control| This is the control bit that is used to indicate that it is a write packet. Its value is 0x09 | | + | |Control| This is the control bit that is used to indicate that it is a read response |
- | |Total length| This indicates the total length of the write packet. It is 4 bytes long| | + | |Total length| This indicates the total length of the read response |
- | |Chip address| This is the address of the chip to which the data has to be written| | + | |Chip address| This is the address of the chip to which the data has been read from| |
|Data Length| This is the length of the data. This is 4 bytes long| | |Data Length| This is the length of the data. This is 4 bytes long| | ||
- | |Address| This is the address of the module whose data is being written to the DSP. This is 2 bytes long| | + | |Address| This is the address of the module whose data has been read from the DSP. This is 2 bytes long| |
|Success / Failure| This byte indicates whether the read operation was a success or failure. It should be populated with a 0 for success and 1 for failure| | |Success / Failure| This byte indicates whether the read operation was a success or failure. It should be populated with a 0 for success and 1 for failure| | ||
|Reserved| This field is reserved for future use| | |Reserved| This field is reserved for future use| | ||
|Data| This is the data read from the address| | |Data| This is the data read from the address| |