This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:sigmastudio:usingsigmastudio:scripting:server [01 Jul 2019 14:52] – Added the ICRegisterRead and Write SigmaServer API's Example Without ICName as Parameter Sanjeeva Reddy | resources:tools-software:sigmastudio:usingsigmastudio:scripting:server [24 Aug 2022 08:28] (current) – Sakthivel Perumal | ||
---|---|---|---|
Line 129: | Line 129: | ||
<code csharp> | <code csharp> | ||
bool DELAY_SCRIPT( int delayMilliseconds ); | bool DELAY_SCRIPT( int delayMilliseconds ); | ||
+ | </ | ||
+ | \\ | ||
+ | \\ | ||
+ | ====SET_TIMEOUT==== | ||
+ | Set SigmaStudio Server API wait timeout for the script. The default timeout set as 30 sec. | ||
+ | <code csharp> | ||
+ | bool | ||
</ | </ | ||
\\ | \\ |