This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:sigmastudio:usingsigmastudio:scripting:iscripted [30 Dec 2022 13:55] – ananthakalyani Sankar | resources:tools-software:sigmastudio:usingsigmastudio:scripting:iscripted [30 Dec 2022 13:56] (current) – [Properties] ananthakalyani Sankar | ||
---|---|---|---|
Line 1733: | Line 1733: | ||
\\ | \\ | ||
\\ | \\ | ||
- | ===== Selfboot Options ===== | + | =====Selfboot Options===== |
===Selfboot Port settings=== | ===Selfboot Port settings=== | ||
<code csharp> | <code csharp> | ||
Line 1817: | Line 1817: | ||
\\ | \\ | ||
====Examples==== | ====Examples==== | ||
- | |||
- | |||
- | """ | ||
- | / | ||
- | * [0] -> EEPROM_MEMORY_SIZE | ||
- | * [1] -> EEPROM_SPI_ADDRESS_BYTES | ||
- | * [2] -> EEPROM_SPI_WRITE | ||
- | * [3] -> EEPROM_SPI_READ | ||
- | * [4] -> EEPROM_SPI_WRITE_ENABLE | ||
- | * [5] -> EEPROM_SPI_ERASE | ||
- | * [6] -> EEPROM_SPI_ERASE_TIME | ||
- | * [7] -> EEPROM_WRITE_SPEED | ||
- | * [8] -> EEPROM_PAGE_SIZE | ||
- | * [9] -> EEPROM_SPI_MODE | ||
- | * [10] -> EEPROM_PROTOCOL | ||
- | * | ||
- | | ||
- | * *************************/ | ||
- | < | ||
- | |||
- | cd C: | ||
- | RegAsm “C: | ||
- | |||
- | cd C: | ||
- | RegAsm “C: | ||
- | |||
- | """ | ||
- | |||
The following shows an example of how to using Selfboot . | The following shows an example of how to using Selfboot . |