This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:tools-software:sigmastudio:usingsigmastudio:schematicversion [07 Jul 2016 08:58] Venkatesan Krishnamoorthy |
resources:tools-software:sigmastudio:usingsigmastudio:schematicversion [08 Aug 2016 14:22] Venkatesan Krishnamoorthy |
||
---|---|---|---|
Line 10: | Line 10: | ||
{{ :resources:tools-software:sigmastudio:usingsigmastudio:versioncontrol.jpg?nolink |}} | {{ :resources:tools-software:sigmastudio:usingsigmastudio:versioncontrol.jpg?nolink |}} | ||
- | There are 2 version numbers, one is major and another minor. The minor can be incremented manually. The major version is incremented whenever there is a change in the schematic (code or parameter change) and the compilation is done. The major version can also be overridden by the user. | + | There are 2 version numbers, one is major and another minor. The minor can be incremented manually. The major version is incremented whenever there is a change in the schematic (code change) and the compilation is done. The major version can also be overridden by the user. |
There is an extra field for "Customer ID" which can be enabled optionally. This is updated manually by the users. | There is an extra field for "Customer ID" which can be enabled optionally. This is updated manually by the users. | ||
The Last three memory locations of DM1 memory are used to maintain these version numbers. | The Last three memory locations of DM1 memory are used to maintain these version numbers. |