Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |
resources:tools-software:sigmastudio:usingsigmastudio:hierarchyboards [19 Jun 2012 15:00] – Approved William Jahn | resources:tools-software:sigmastudio:usingsigmastudio:hierarchyboards [03 Jan 2013 20:42] (current) – external edit 127.0.0.1 |
---|
| |
| |
<note>Note: It is possible to create nested hierarchy boards (a hierarchy board with-in another hierarchy board's tab). To create a nested board, first select a hierarchy tab at the bottom of the Schematic window, then drag-and-drop a hierarchy board block. If you hover the mouse button over a board tab, the tool-tip will display the "path" of the board (the location of the board block relative to Main). This is helpful when several board's have the same name, which is common when using board files.</note> | <WRAP round help>Note: It is possible to create nested hierarchy boards (a hierarchy board with-in another hierarchy board's tab). To create a nested board, first select a hierarchy tab at the bottom of the Schematic window, then drag-and-drop a hierarchy board block. If you hover the mouse button over a board tab, the tool-tip will display the "path" of the board (the location of the board block relative to Main). This is helpful when several board's have the same name, which is common when using board files.</WRAP> |
{{ hierarchypic3.png }}\\ | {{ hierarchypic3.png }}\\ |
\\ | \\ |