This is an old revision of the document!
Right clicking on Input Alias will show option to Add output Alias. That output Alias can be moved to anywhere in schematic and connected with any block as signal destination. One Input Alias can have multiple output Aliases if required.
Clicking on any Input/Output Alias will highlight All Aliases. Output Aliases will be highlighted in “Aqua” color and Input Alias will be highlighted in “Orange” color.
User can go to particular output alias of choice by using this option. Example: If user clicks “1” in Goto CouterPart Alias option, then “FIR1” block will come into center part of schematic even if it is not in visible area of schematic. This helps user to easily navigate between and evaluate the schematic design.
At any time, user can navigate back to Input Alias from any Output Alias using this option. Goto Input Alias option will be shown in every output alias. After clicking that option, Input Alias block will come into center part of schematic even if it is not in visible area of schematic. This helps user to easily navigate between and evaluate the schematic design.