Click here to return to the Volume Controls section.
This module applies mute to the input when enabled. When the module is grown the mute selection is separate for each of the inputs. It comes in two versions.
HW slew version shall apply the slew whenever mute parameter is changed to avoid click noise.
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Input | dec- audio | Input Audio |
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 1: Output | dec- audio | Output audio with gain. |
The module currently supports growth. Both the control and pins are grown for each growth. Add algorithm functionality is not supported. The figure below shows the module when grown for 5 channels.
GUI Control Name | Default Value | Range | Function Description |
---|---|---|---|
Gain* | 1 | -128 to 127.999 | Gain value in linear scale. |
Note: Gain control will be repeated for each channels when grown.
In the case of HW slew version. The slew shape can be chosen by right clicking on the module.
GUI Control Name | Compiler Name | Function Description |
---|---|---|
Mute | MultipleControlGainS300Alg1mute0 | Mute Selection (0.0/1.0) |
Here,
GUI Control Name | Compiler Name | Function Description |
---|---|---|
Slew Mode | MultipleControlGainHWSelwAlg1slew_mode | HW Slew Mode |
Mute | MultipleControlGainHWSelwAlg1mute0 | Mute Selected or not (0.0/1.0) |
Here,
Note: Mute parameter shall be repeated for each channel when the algorithm is grown.