This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:tools-software:sigmastudio:toolbox:sources:vco [21 Jun 2012 22:46] – created Brett Gildersleeve | resources:tools-software:sigmastudio:toolbox:sources:vco [02 Jun 2021 15:44] (current) – Clarify number format and ranges, add example schematic Joshua Berlin | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | <WRAP center round todo 60%> | + | ====== Voltage Controlled Oscillator ====== |
- | Under Construction | + | |
- | </ | + | |
+ | [[: | ||
+ | |||
+ | The Voltage Controlled Oscillator block is typically used for modulation applications. The block has a control input signal (orange pin) which specifies a frequency. The blue pin generates a sine tone at the appropriate frequency. | ||
+ | {{ : | ||
+ | \\ \\ | ||
+ | The input value may be from zero to one (5.23 format, or on ADAU145x/ | ||
+ | |||
+ | The VCO accepts values from 0 Hz (0.0 input) to Fs/2 (1.0 input). Fs is the sampling frequency. The algorithm linearly interpolates the input value into an output frequency. | ||
+ | \\ \\ | ||
+ | Note that if the input is greater than 1, the derived output value will fold back to frequencies below Fs/2. | ||
+ | \\ \\ | ||
+ | === Example Schematic === | ||
+ | {{ : |