Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Next revision
Previous revision
resources:tools-software:sigmastudio:toolbox:sources:vco [21 Jun 2012 22:46] – created Brett Gildersleeveresources:tools-software:sigmastudio:toolbox:sources:vco [02 Jun 2021 15:44] (current) – Clarify number format and ranges, add example schematic Joshua Berlin
Line 1: Line 1:
-<WRAP center round todo 60%> +====== Voltage Controlled Oscillator ======
-Under Construction +
-</WRAP>+
  
 +[[:resources:tools-software:sigmastudio:toolbox:sources|Click here to return to the Sources section.]]
 +
 +The Voltage Controlled Oscillator block is typically used for modulation applications. The block has a control input signal (orange pin) which specifies a frequency. The blue pin generates a sine tone at the appropriate frequency.
 +{{ :resources:tools-software:sigmastudio:toolbox:sources:vco003.jpg}}
 +\\ \\
 +The input value may be from zero to one (5.23 format, or on ADAU145x/ADAU146x, 8.24 format).
 +
 +The VCO accepts values from 0 Hz (0.0 input) to Fs/2 (1.0 input). Fs is the sampling frequency. The algorithm linearly interpolates the input value into an output frequency.
 +\\ \\
 +Note that if the input is greater than 1, the derived output value will fold back to frequencies below Fs/2.
 +\\ \\
 +=== Example Schematic ===
 +{{ :resources:tools-software:sigmastudio:toolbox:sources:vco_sigmastudio_project.png?nolink |}}
resources/tools-software/sigmastudio/toolbox/sources/vco.txt · Last modified: 02 Jun 2021 15:44 by Joshua Berlin