This is an old revision of the document!
Click here to return to the Sources section.
The Tone (Lookup/Sine) block generates a tone from a lookup table. The gain and the initial phase of the algorithm can be configured. Set the tone frequency in text field or use the arrows; the checkbox turns the tone on and off.
To change the source's Sampling Rate, Right-click in the block and select Set Sampling Rate, which will open the Sampling Rate window (default is 44.1 kHz).
GUI Control Name | Default Value | Range | Function Description |
---|---|---|---|
on/off | off | on/off | Turns the output of the cell on or off. When the output is off, the output pin will output a constant value of 0. |
Frequency | 500.01 | 0.01 to 0.5*Sample Rate | The sets the frequency of the sine tone that is output from the cell. |
Initial Phase | 0 | 0 to 360 | Initial Phase of the sine signal. |
Gain | 0 | -144 to 42 dB | The gain to be multiplied on the sine tone |