This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:tools-software:sigmastudio:toolbox:sources:beepsources [21 Jun 2012 22:49] – created Brett Gildersleeve | resources:tools-software:sigmastudio:toolbox:sources:beepsources [02 Aug 2012 21:01] (current) – Added return link Brett Gildersleeve | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | <WRAP center round todo 60%> | + | ====== Beep ====== |
- | Under Construction | + | |
- | </ | + | |
+ | [[: | ||
+ | |||
+ | |This block uses an internal oscillator to generate tones. Set the frequency in the text field or using the arrows. | ||
+ | \\ | ||
+ | \\ | ||
+ | You can add algorithms to the Beep blocks after the default has been established (if you're using more than one DSP processor, you'll need to add the initial default algorithm for the desired IC). Right-click the block to select Add Algorithm > IC # > Beep variable gain and add another output pin. | ||
+ | \\ | ||
+ | \\ | ||
+ | To change the source' | ||
+ | |||
+ | ===== Usage ===== | ||
+ | |||
+ | For most applications we recommend using Tone (Lookup/ | ||
+ | \\ | ||
+ | \\ | ||
+ | Beep is most valuable for schematic testing as it produces less THD than the Tone (lookup/ |