This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:tools-software:sigmastudio:toolbox:multirateprocessing:upsampling [21 Dec 2016 11:23] – Venkatesan Krishnamoorthy | resources:tools-software:sigmastudio:toolbox:multirateprocessing:upsampling [12 May 2017 14:23] – Suhasini Raghuram | ||
---|---|---|---|
Line 6: | Line 6: | ||
\\ | \\ | ||
\\ | \\ | ||
- | {{ : | + | {{ : |
\\ | \\ | ||
- | **Note:** Module does not do the low pass filtering after increasing the samples. It is the users responsibility to add a low pass filter after the up-sampling. | + | |
===== Input Pins ===== | ===== Input Pins ===== | ||
Line 27: | Line 27: | ||
^GUI Control Name^Default Value^Range^Function Description^ | ^GUI Control Name^Default Value^Range^Function Description^ | ||
|Upsample Factor|2| 2, | |Upsample Factor|2| 2, | ||
+ | |LPF|Checked|Checked/ | ||
The upsampler can either insert zeros or repeat the previous sample(Zero Order Hold) during upsampling. This can be configured in the contex menu. | The upsampler can either insert zeros or repeat the previous sample(Zero Order Hold) during upsampling. This can be configured in the contex menu. | ||
{{ : | {{ : | ||
- | Change in the ' | + | Change in the ' |
\\ | \\ | ||
=====DSP Parameter Information===== | =====DSP Parameter Information===== |