This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudio:toolbox:multirateprocessing:synchronoussrc [06 Nov 2017 13:05] – Prasad Kamath | resources:tools-software:sigmastudio:toolbox:multirateprocessing:synchronoussrc [08 Apr 2019 16:09] (current) – edited description to make content more clear Prasad Kamath | ||
---|---|---|---|
Line 43: | Line 43: | ||
==== Up sampling ==== | ==== Up sampling ==== | ||
\\ | \\ | ||
- | The module acts as an upsampler when the output sample rate is greater than the input sample rate. The following example interpolates the input signal which is a sine tone of 500Hz sampled at 44.1 KHz to an output sine tone at 500Hz sampled at the output sampling frequency of 48KHz. | + | The module acts as an upsampler when the output sample rate is greater than the input sample rate. The following example interpolates the input signal which is a sine tone of 500Hz sampled at 44.1 KHz to an output sine tone at 500Hz sampled at the output sampling frequency of 48KHz. |
\\ | \\ | ||
{{ : | {{ : | ||
Line 51: | Line 51: | ||
\\ | \\ | ||
- | The module acts as an down sampler when the input sample rate is greater than the output sample rate. The following example interpolates the input signal which is a sine tone of 800Hz sampled at 48 KHz to an output sine tone at 800Hz sampled at the output sampling frequency of 44.1KHz. | + | The module acts as an down sampler when the input sample rate is greater than the output sample rate. The following example interpolates the input signal which is a sine tone of 800Hz sampled at 48 KHz to an output sine tone at 800Hz sampled at the output sampling frequency of 44.1KHz. Here tone1_2 is set to a sampling rate of 48khz tone1_3 is set to a sampling rate of 44.1khz. |
\\ | \\ | ||
{{ : | {{ : | ||
\\ | \\ | ||
+ | <WRAP center round info 100%> | ||
+ | Note: The output pins of the Sample rate converter must always be connected. If the module is placed at the end of the signal chain, connect the output pins to the output modules. | ||
+ | </ | ||
==== Down sampling - Up sampling ==== | ==== Down sampling - Up sampling ==== |