Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:tools-software:sigmastudio:toolbox:multirateprocessing:downsampling [12 May 2017 14:21]
Suhasini Raghuram [Down Sampling]
resources:tools-software:sigmastudio:toolbox:multirateprocessing:downsampling [04 Jan 2021 06:14]
Sanjeeva Reddy Updated Downsample image
Line 3: Line 3:
 \\ \\
 \\ \\
-The down sampling module is mainly used to get the input samples to a lower sampling rate and process.For example the bass portion of the audio need not be processed at higher sampling rates as the frequencies associated with bass are low.+The down sampling module is mainly used to get the input samples to a lower sampling rate and process. For example the bass portion of the audio need not be processed at higher sampling rates as the frequencies associated with bass are low.
    
 This module takes the downsample factor from the GUI parameters and down sample the input accordingly. ​ This module takes the downsample factor from the GUI parameters and down sample the input accordingly. ​
 \\ \\
 \\ \\
-{{ :​resources:​tools-software:​sigmastudio:​toolbox:​multirateprocessing:​downsampler.png?nolink |+{{ :​resources:​tools-software:​sigmastudio:​toolbox:​multirateprocessing:​downsamping4p6.png?nolink |}} 
 +\\
 \\ \\
- 
-\\}} 
 ===== Input Pins ===== ===== Input Pins =====
 ^Name^Format [int/dec] - [control/​audio]^Function Description^ ^Name^Format [int/dec] - [control/​audio]^Function Description^
Line 25: Line 24:
 ^GUI Control Name^Default Value^Range^Function Description^ ^GUI Control Name^Default Value^Range^Function Description^
 |Downsample Factor|2| 2,​3,​4,​6,​8,​16 |The factor at with the input sample rate will be divided| |Downsample Factor|2| 2,​3,​4,​6,​8,​16 |The factor at with the input sample rate will be divided|
-|LPF|Checked|Checked/​Unchecked|If checked, an anti aliasing filter will be applied before downsampling the signal| 
  
 Change in GUI configuration needs a recompilation of the schematic. ​ Change in GUI configuration needs a recompilation of the schematic. ​
resources/tools-software/sigmastudio/toolbox/multirateprocessing/downsampling.txt · Last modified: 04 Jan 2021 06:14 by Sanjeeva Reddy