This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:stereswitchnx2 [21 Jun 2012 22:35] – created Brett Gildersleeve | resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:stereswitchnx2 [03 Aug 2012 17:34] (current) – Added link Brett Gildersleeve | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | <WRAP center round todo 60%> | + | ====== Stereo Switch Nx2 ====== |
- | Under Construction | + | |
- | </ | + | |
+ | [[resources/ | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | Use the radio buttons in this multichannel block to select between or among sets of stereo inputs and send one set to one of the (2-channel) outputs. | ||
+ | |||
+ | To begin, drag the block into the workspace, right-click it and select Add Algorithm > IC N Stereo/Slew or Stereo. (The result appears the same either way.) The 2 Channel/ | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | The default block (above right) is ready to use as a 2x1 connection, and like the others can be grown by right-clicking to select your desired number of input sets. | ||
+ | |||
+ | See the Multiplexer/ |