This shows you the differences between two versions of the page.
Last revisionBoth sides next revision | |||
resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:stereoswitch2xn [21 Jun 2012 22:35] – created Brett Gildersleeve | resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:stereoswitch2xn [03 Aug 2012 17:13] – Created Brett Gildersleeve | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | <WRAP center round todo 60%> | + | ====== Stereo Switch 2xN ====== |
- | Under Construction | + | |
- | </ | + | |
+ | Route a stereo input to one of several possible stereo outputs with this block, using the strip of radio button pairs to select which output. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | To begin, drag the block into the workspace, right-click it and select Add Algorithm > IC N Stereo/Slew or Stereo. (The result appears the same; this default is shown at top right.) The Stereo/Slew algorithm lets you rapidly ramp the stereo source level up and down without any clicking noises when switching among the stereo outputs. It uses N hardware volume controls in the target/slew RAM to do the job. | ||
+ | |||
+ | The default block shown above right is ready to use as a 2x4 connection, and like the others can be grown by right-clicking to select your desired number of stereo outputs. Below the default at right is a block grown by 3 (3 pairs, equaling 6, totaling 10). |