This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:monoswitch1xn [21 Jun 2012 22:36] – created Brett Gildersleeve | resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:monoswitch1xn [03 Aug 2012 17:38] (current) – Added link Brett Gildersleeve | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | <WRAP center round todo 60%> | + | ====== Mono Switch 1xN ====== |
- | Under Construction | + | |
- | </ | + | |
+ | [[resources/ | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | The Mono Switch block routes an input signal to one of many possible outputs, the strip of radio buttons is used to select an output (each radio button corresponds to a coefficient RAM parameter). | ||
+ | |||
+ | To begin, drag the block into the workspace, right-click it and select Add Algorithm > IC N Mono/Slew or Mono. (The result appears the same.) The Mono/Slew algorithm lets you rapidly ramp the source level up and down without any clicking noises when switching outputs. It uses N hardware volume controls in the target/slew RAM to do its job. | ||
+ | |||
+ | See the Multiplexer/ | ||
+ | |||
+ | The default block is ready to use as a 1x2 connection, and like the others can be grown by right-clicking and selecting the desired number of outputs. The example below has been grown by 3: | ||
+ | |||
+ | {{ : |