This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:indexselectablemultiplexer [21 Jun 2012 22:36] – created Brett Gildersleeve | resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:indexselectablemultiplexer [03 Aug 2012 17:39] (current) – Added link Brett Gildersleeve | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | <WRAP center round todo 60%> | + | ====== Index Selectable Multiplexer ====== |
- | Under Construction | + | |
- | </ | + | |
+ | [[resources/ | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | This block routes the signal from either of its two input pins, based on the control signal input index value from the Index Lookup Table, RMS Table or DC Input. | ||
+ | |||
+ | See the Multiplexer/ | ||
+ | |||
+ | Drag the block into the workspace and right-click to select Add Algorithm > IC # > Mono/ | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | Like its companion blocks, this block can be grown. Right-click and select Grow Algorithms from the context menu. Growing will create additional input pins, single pins with the Mono algorithm, stereo input pin pairs with the Stereo algorithm. To select a particular input signal, set the control signal to an input pin's integer index starting from 0, using a 28.0 format integer value. | ||
+ | |||
+ | {{ : |