The Balance fader blocks is used to adjust the strength of the audio level between the left and right channels and fade out of the audio level between the front and rear channels.
Name | ADSP-214xx | ADSP-215xx/SC5xx | ADAU145x/146x |
---|---|---|---|
Balance Fader | NA | Block | NA |
Name | Type | Description |
---|---|---|
FrontRight_Input | Audio | Front right channel input to the balance fader |
FrontLeft_Input | Audio | Front left channel input to the balance fader |
RearRight_Input | Audio | Rear right channel input to the balance fader |
RearLeft_Input | Audio | Rear left channel input to the balance fader |
Center_Input | Audio | Center channel input to the balance fader |
SW_Input | Audio | Sub woofer input to the balance fader |
Name | Type | Description |
---|---|---|
FrontRight_Output | Audio | Front right channel output from the balance fader |
FrontLeft_Output | Audio | Front left channel output from the balance fader |
RearRight_Output | Audio | Rear right channel output from the balance fader |
RearLeft_Output | Audio | Rear left channel output from the balance fader |
Center_Output | Audio | Center channel output from the balance fader |
SW_Output | Audio | Sub woofer output from the balance fader |
GUI Parameter Name | Default Value | Range | Function Description |
---|---|---|---|
Balance | 0 | -10 to 10 | Controls the balance of audio level between the left and right channels |
Fade | 0 | -10 to 10 | Controls the fade out of audio level between the front and rear channels. |
StepSize | 11 | 8 to 16 | Controls the smooth transition of change in audio level |
Parameter Name | Description | ADSP-214xx/SC5xx/215xx | ADAU145x/146x |
---|---|---|---|
Balance | Balance of audio level between the left and right channels | Float | NA |
Fade | Fade out of audio level between the front and rear channels | Float | NA |
StepSize | Allows smooth transition of change in audio level | Float | NA |
BalanceFadeDBVal | Constant values | Float | NA |