Click here to return to the Level Detectors Lookup Tables
| This block functions like the Index Lookup Table, except now there is a matrix of values in the table. The size of the table is user determined. There are two inputs, one for the Y index and one for the X index. | ![]() |
Here is an example of a 4×4 table.
Description: For this algorithm, the inputs are the index value X(column) and index value Y(row) into the LUT. By default the module expect the index to be in integer format 32.0. [0][0] will index the first value in the table. The default output format is fractional 8.24.
There are two versions of this algorithm.