This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:tools-software:sigmastudio:toolbox:io:output [08 Aug 2012 17:13] – [ADAU1761] Fixed table, showing the DACs are available regardless of serial port setting. Brett Gildersleeve | resources:tools-software:sigmastudio:toolbox:io:output [19 Apr 2017 07:13] – [Input Pins] Suhasini Raghuram | ||
---|---|---|---|
Line 112: | Line 112: | ||
===== AD1953 Output ===== | ===== AD1953 Output ===== | ||
- | <note warning>The AD1953 is not recommended for new designs. Information is included here for reference only.</note> | + | <WRAP alert>The AD1953 is not recommended for new designs. Information is included here for reference only.</WRAP> |
The AD1953 has the DACs built into the DSP core, so you must choose an interpolation filter for the output. To use Output blocks with the AD1953 you will need to add an algorithm. As shown below, right-click the block to select which interpolating filter you would like to implement in the DSP core.\\ | The AD1953 has the DACs built into the DSP core, so you must choose an interpolation filter for the output. To use Output blocks with the AD1953 you will need to add an algorithm. As shown below, right-click the block to select which interpolating filter you would like to implement in the DSP core.\\ | ||
Line 150: | Line 150: | ||
50dB interpolation filter. Flat to 20kHz with a 48kHz sample rate; uses 53 instructions. | 50dB interpolation filter. Flat to 20kHz with a 48kHz sample rate; uses 53 instructions. | ||
+ | ===== ADAU145x Output ===== | ||
+ | ====Input Pins ==== | ||
+ | ^Name^Format \\ [int/dec] - [control/ | ||
+ | |Pin 0: Input|dec- audio|The data to be written to output register| | ||
+ | |||
+ | ==== Grow Algorithm ==== | ||
+ | This output module supports growth upto 16 channels. The output algorithm will be optimized to reduce MIPS when the grown output channels are consecutive and the starting index is a multiple of 4. | ||
+ | |||
+ | ==== Relationship Between Hardware Outputs and SigmaStudio Output Channels ==== | ||
+ | The relationship between an output cell in SigmaStudio and the physical output pin on the chip can vary in some cases depending on register settings. Refer to //Serial Audio Outputs from DSP Core// section in the [[http:// |