This is an old revision of the document!
Click here to return to the IO page
The Input block receives input from the hardware's input pins and makes it available in the schematic design.
To enable/disable an input:
Check the block for the input channel(s) you with to enable. Un-check the box disable an input channel. The pin will turn blue when an input is enabled and grey when disabled. The default block has two pins enabled, for stereo connection.
If you have multiple DSP processors in your design, specify which DSP is associated with the input block by right-clicking and selecting Add Algorithm > IC # > DSP Type.
For SigmaDSP products that only have digital audio inputs, the routing is quite simple. Each checkbox on the input cell corresponds to one input channel. Because TDM modes can be used, the exact mapping between a hardware pin and corresponding input channels will change based on the register configuration.
For SigmaDSP products that contain both analog and digital inputs, the analog inputs are represented on the top portion of the input cell and the digital inputs occupy the remaining positions on the input cell. For example, on the ADAU170x and ADAU1761 devices, which have two ADC input channels, the left ADC corresponds to input channel 0, the right ADC corresponds to input channel 1, and the digital I2S/TDM channels correspond to channels 2 through 9 on the input cell.
For the ADAU1701 (and ADAU1702, ADAU1401, ADAU1401A), which have 2 analog channels and up to 8 digital channels, the input channels are routed as follows:
Hardware Input | Channel Assignment in Input Block |
---|---|
Left ADC | 0 |
Right ADC | 1 |
First channel in I2S or TDM stream | 2 |
Second channel in I2S or TDM stream | 3 |
Third channel in I2S or TDM stream | 4 |
Fourth channel in I2S or TDM stream | 5 |
Fifth channel in I2S or TDM stream | 6 |
Sixth channel in I2S or TDM stream | 7 |
Seventh channel in I2S or TDM stream | 8 |
Eighth channel in I2S or TDM stream | 9 |
For the ADAU1761, the routing is dependent on the channel settings of the serial port.
Hardware Input | Channel Assignment in Input Block |
---|---|
Left ADC | 0 |
Right ADC | 1 |
First channel in I2S stream | 2 |
Second channel in I2S stream | 3 |
Hardware Input | Channel Assignment in Input Block |
---|---|
Left ADC | 0 |
Right ADC | 1 |
First channel in I2S or TDM stream | 2 |
Third channel in I2S or TDM stream | 3 |
Second channel in I2S or TDM stream | 4 |
Fourth channel in I2S or TDM stream | 5 |
Hardware Input | Channel Assignment in Input Block |
---|---|
Left ADC | 0 |
Right ADC | 1 |
First channel in I2S or TDM stream | 2 |
Fifth channel in I2S or TDM stream | 3 |
Second channel in I2S or TDM stream | 4 |
Sixth channel in I2S or TDM stream | 5 |
Third channel in I2S or TDM stream | 6 |
Seventh channel in I2S or TDM stream | 7 |
Fourth channel in I2S or TDM stream | 8 |
Eighth channel in I2S or TDM stream | 9 |