This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:tools-software:sigmastudio:toolbox:gpioconditioning:pushbuttonvolume [02 Aug 2012 17:12] – Added content from help file William Jahn | resources:tools-software:sigmastudio:toolbox:gpioconditioning:pushbuttonvolume [02 Aug 2012 17:20] – format adjustment William Jahn | ||
---|---|---|---|
Line 11: | Line 11: | ||
===Input Pins=== | ===Input Pins=== | ||
- | |Name|Format \\ [int/dec] - [control/ | + | |**Name**|**Format \\ [int/dec] - [control/ |
|Pin 0: PushButton Up|int - control|GPIO signal from Pushbutton that increases the volume| | |Pin 0: PushButton Up|int - control|GPIO signal from Pushbutton that increases the volume| | ||
|Pin 1: PushButton Down|int - control|GPIO signal from Pushbutton that decreases the volume| | |Pin 1: PushButton Down|int - control|GPIO signal from Pushbutton that decreases the volume| | ||
Line 18: | Line 18: | ||
===Output Pins=== | ===Output Pins=== | ||
- | |Name|Format \\ [int/dec] - [control/ | + | |**Name**|**Format \\ [int/dec] - [control/ |
|Pin 0: Interface Write|n/ | |Pin 0: Interface Write|n/ | ||
|Pin 1: Output Audio|decimal - audio|Volume adjusted audio output| | |Pin 1: Output Audio|decimal - audio|Volume adjusted audio output| | ||
===GUI Controls=== | ===GUI Controls=== | ||
- | |GUI Control Name|Default Value|Range|Function Description| | + | |**GUI Control Name**|**Default Value**|**Range**|**Function Description**| |
|Invert GPIO|unchecked|[checked, | |Invert GPIO|unchecked|[checked, | ||
|Hold (ms)|500|[0, | |Hold (ms)|500|[0, | ||
Line 32: | Line 32: | ||
===DSP Parameter Information=== | ===DSP Parameter Information=== | ||
- | |GUI Control Name|Compiler Name|Function Description| | + | |**GUI Control Name**|**Compiler Name**|**Function Description**| |
|Hold (ms)|PushButtonVolAlg1holdtime|The hold time is written to the DSP as the number of samples representing the millisecond time: Samples = < | |Hold (ms)|PushButtonVolAlg1holdtime|The hold time is written to the DSP as the number of samples representing the millisecond time: Samples = < | ||
|Repeat (ms)|PushButtonVolAlg1repeattime|The release time is written to the DSP as the number of samples representing the millisecond time: Samples = < | |Repeat (ms)|PushButtonVolAlg1repeattime|The release time is written to the DSP as the number of samples representing the millisecond time: Samples = < |