This is an old revision of the document!
Click here to return to the basicdsp page
This Module computes the Gain of the Compressor. Compression happens by taking the RMS of the Average of all inputs, and then looking up for the Gain based on the Compressor Graph.
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Input | decimal - Audio | Audio Input |
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Output | decimal - Audio | Gain Output |
The module supports Input Channel growth upto a maximum of 6 channels.
Compressor graph has a “Point Density” context menu option for varying the resolution of the Points in the compressor graph. 288(0.5db), 720(0.2db) and 1440(0.1db) are the Point densities supported.
GUI Control Name | Default Value | Range | Function Description | ||||
---|---|---|---|---|---|---|---|
RMSTC | 121 | 1 – 8686 db/s | Determines how rapidly the compressor will respond to input signal level changes | Hold | 0 | 0-2000 | Controls the time (in ms) the compressor maintains its current output gain setting before it starts decreasing as the input level decrease. |
Decay | 10 | 1 - 8686 db/s | Controls the rate at which the compressor gain decreases in response to decrease in the input signal level. | ||||
Soft-knee | - | - | Soft-knee lets the compressor ease into action, making a less-abrupt change from unprocessed signal to compressed signal. | ||||
Graph | - | - | Compression Editor Graph. |
GUI Control Name | Compiler Name | Function Description |
---|---|---|
RMSTC |