This is an old revision of the document!
Click here to return to the Basic DSP page
Scalar Addition is a block processing module which adds a constant scalar value to each of the input
samples in block of input samples
Name | Format [int/dec/float] - [control/audio] | Function Description |
---|---|---|
Pin 0: Input | decimal(ADAU145x)- audio | Input signal to the module |
Name | Format [int/dec/float] - [control/audio] | Function Description |
---|---|---|
Pin 0: Output | decimal(ADAU145x)- audio- audio | Output signal from the module |
The module supports growth functionality, the number of channels to the module can be grown. Add is not supported.
GUI Control Name | Default Value | Range | Function Description |
---|---|---|---|
Scalar | 1 | -128-127.99 | Scalar Value used for addition with input block of samples |
GUI Control Name | Compiler Name | Function Description |
---|---|---|
Scalar | ScalarAdditionBlkAlg2Scalar | Scalar Value for Addition |
This module adds the scalar value specified in the textbox to each of the input samples in an
input block.
In the example shown below, scalar value 110 is added to each of the DC block input samples of value 10
1. ADAU145x